(1)| 1/29/2020 11:14 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello aylar; To my knowledge, Modbus TCP servers must be distinguished by unique IP addresses, as well as unique Modbus node addresses to be recognized by the Modbus TCP client. See this article for details: https://control.com/forums/threads/slave-id-importance-in-modbus-tcp-ip.43750/ You should look for a way to change the equipment's IP address. Hope this helps, |
| 1/30/2020 7:31 AM | |
|
Posts: 6 Rating:
|
OK But this device is gateway for Lora module like as converter for modbus RTU to TCP/IP and couldn't produce several IP for each slave . thanks |
| 1/30/2020 7:42 AM | |
|
Joined: 10/3/2010 Last visit: 1/22/2026 Posts: 1572 Rating:
|
Most drivers understand configuration of Modbus slaves address like example below: "192.168.6.127,8" "192.168.6.127:8" "192.168.6.127@8" where 8 is the slave ID Something similar should be available |
|
B r g d s , |
|
| 1/30/2020 10:32 AM | |
|
Posts: 6 Rating:
|
but in wincc how can i write like this format ? |
| 1/30/2020 1:01 PM | |
|
Joined: 10/3/2010 Last visit: 1/22/2026 Posts: 1572 Rating:
|
there's an input field in the properties for the remote slave address |
|
B r g d s , |
|
This contribution was helpful to
|
|
| 2/28/2024 10:41 AM | |
|
Joined: 8/12/2016 Last visit: 12/23/2025 Posts: 109 Rating:
|
I am facing the same problem. Did you find a way to deal with the issue you had? |
Follow us on