3/13/2024 12:54 PM | |
Joined: 11/25/2023 Last visit: 7/29/2025 Posts: 1 Rating:
|
Hi all, Is it possible to Assign PLC address from the unified comfort panel (e.g. MTP 700) when I have set in my project PLC as "IP Address is set directly at the device". I know there is a T_CONFIG for PLC, and that works fine from the HMI, but if I change that way the address of PLC, how can I make a connection? Is there somewhere "set connection" as it is in KTP/TP panels? What I'm looking for is : https://support.industry.siemens.com/cs/sk/en/view/67653385 Thank you. Maros. |
Follow us on