3/15/2024 11:07 AM | |
Joined: 2/16/2024 Last visit: 6/13/2024 Posts: 2 Rating: (0) |
Hi sir Want to know can we connect dvp plc with Siemens plc I have Siemens 1513 1pn CPU and already working with system which is running with et200 setup want to read data from CPU direct with delta plc for checking some parameters is it possible if we connect delta 12se plc with ethernet on switch already connected with Siemens plc CPU ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/18/2024 05:16:56New subject after splitting |
|
3/18/2024 7:46 AM | |
Joined: 7/9/2015 Last visit: 5/29/2024 Posts: 3850 Rating: (565)
|
Hi, I do not know the specification of this DVP PLC. But the S7-1500 can be connected as an I-Device, for example, or it could also communicate via TCPIP using Open User Communication. So please check this manual for S7-1500: SIMATIC S7-1500, ET 200MP, ET 200SP, ET 200AL, ET 200pro, ET 200eco PN CommunicationRegards, Towome
|
|
|
Follow us on