3/27/2024 6:18 PM | |
Joined: 9/15/2021 Last visit: 8/5/2025 Posts: 4 Rating:
|
Hello, are there any news on this topic with Unified RT V18? the .bat (or .cmd) file solution works fine with using the OpenPipe feature but only outside the kiosk mode. Using the Win10 kiosk mode with Edge doesn't allow anything running in the background and seemingly blocks the autostart-folder content as well (required for OpenPipe). Using a UPS with interface or less restrictive blocking of windows are no options. Possibly the "SIMATIC WinCC Unified Station Configurator V19" (109771719) brings a solution but we're still on V18 on this machine. Thanks if anybody has an idea! |
Follow us on