1/19/2024 12:20 PM | |
Joined: 5/21/2015 Last visit: 12/4/2024 Posts: 1 Rating:
|
Hi Experts Need your Support I am using WINCC V8.0 as a OPC UA Client and Redlion Gateway DA30 as OPC UA server. Both are in the same subnet. No username, password and security certificates are set for OPC UA in both WinCC and Redlion, since Redlion uses "None" Security as default. I am able to browse, read and write the OPC tags of Redlion DA30 via UA expert OPC browser and Kepware as OPC UA client. But when I try from WinCC V8.0 I am able to create the OPC UA Channel adapter and browse the tags of Redlion DA30 Gateway, when I try to use the browsed tag in the WinCC Tag Management it Shows an error as below ------ >> 0x04 - bad - configuration error (value not accepted) " under quality code and the Tag Value is "0" <<-------- I checked with the WinCC diagnose logs files for OPC UA Channel and forund the below message ------------------------------------------------>><<>><<-------------------------------------------------------------------- 2024-01-19 17:23:57,036 INFO Log starting ... 2024-01-19 17:23:57,036 INFO | LogFileName : C:\Program Files (x86)\Siemens\WinCC\Diagnose\OPC_UA_WinCC_Channel_01.LOG 2024-01-19 17:23:57,036 INFO | LogFileCount : 3 2024-01-19 17:23:57,036 INFO | LogFileSize : 1400000 2024-01-19 17:23:57,036 INFO | TraceFlags : c4000000 2024-01-19 17:23:57,036 INFO | Process-ID : 000045b8 2024-01-19 17:23:57,036 INFO Process (PID: 17848 | C:\PROGRAM FILES (X86)\SIEMENS\WINCC\BIN\CCDMRTCHANNELHOST_X64.EXE) attached at 2024-01-19 11:53:57,036 UTC 2024-01-19 17:23:57,179 INFO ServerUri: opc.tcp://192.168.27.100:4840 SecurityMode : None SecurityPolicy : http://opcfoundation.org/UA/SecurityPolicy#None UserIdentityToken: AnonymousIdentityToken 2024-01-19 17:23:57,179 INFO ServerUri: opc.tcp://SERVER01-SRI:53530/OPCUA/SimulationServer SecurityMode : None SecurityPolicy : http://opcfoundation.org/UA/SecurityPolicy#None UserIdentityToken: AnonymousIdentityToken 2024-01-19 17:23:57,481 INFO < CConnection::SetEnabled(): Connection "Edge_GW" state changed to ENABLED 2024-01-19 17:23:57,481 ERROR IConnection: RegisterVariables failed completely [hr=0x80004005] for Connection Edge_GW 2024-01-19 17:23:57,481 INFO < CConnection::SetEnabled(): Connection "Test46" state changed to ENABLED 2024-01-19 17:23:57,481 ERROR CConnection::SetHResultErrorToDiag() Edge_GW from RegisterVariables [hr=0x80004005] 2024-01-19 17:23:57,481 ERROR IConnection: RegisterVariables failed completely [hr=0x80004005] for Connection Test46 2024-01-19 17:23:57,481 ERROR CConnection::SetHResultErrorToDiag() Test46 from RegisterVariables [hr=0x80004005] 2024-01-19 17:23:57,605 INFO ServerUri: opc.tcp://192.168.27.100:4840 SecurityMode : opc.tcp://192.168.27.100:4840 SecurityPolicy : opc.tcp://192.168.27.100:4840 UserIdentityToken: opc.tcp://192.168.27.100:4840 2024-01-19 17:24:07,675 SUCCESS Connection Name "Edge_GW" status OK 2024-01-19 17:24:20,485 ERROR GetData():Empty Value type for Variable LINE1_PM_01_MACHINE_STATUS in Connection Edge_GW 2024-01-19 17:24:20,485 ERROR GetData():Empty Value type for Variable LINE1_PM_01_PRDN_COUNT in Connection Edge_GW 2024-01-19 17:24:50,236 INFO Process (PID: 17848 | C:\PROGRAM FILES (X86)\SIEMENS\WINCC\BIN\CCDMRTCHANNELHOST_X64.EXE) detached at 2024-01-19 11:54:50,236 UTC ------------------------------------------------>><<>><<----------------------------------------------------------------- I did try connecting WinCC V8.0 as OPC UA client with Pryosys OPC UA Simulator and Kepware OPC UA Simulators and these OPC servers works fine and I am able to read and write the OPC tags without any errors. Kindly help in finding a solution AttachmentOPC_UA_WinCC_Channel.txt (565 Downloads) |
Follow us on