6/26/2024 4:40 PM | |
Joined: 11/8/2017 Last visit: 8/23/2025 Posts: 355 Rating:
|
Hi, You can use 'direct addressing' to read / write values from / to devices that are on different UDP ports. Refer to the attached PDF - examples are provided towards the end of the document on Page 74. For your scenario, the second example in the IP/IP section is what you should look at. The addressing syntax that is referred to is entered into the 'Edit I/O addresses' section of the controller when in the CFC tool. No additional hardware is required. Regards, AttachmentCM110666_A6V12019002_en.pdf (533 Downloads) |
Last edited by: CJ. at: 06/26/2024 16:41:13Last edited by: CJ. at: 06/26/2024 16:51:18 |
|
This contribution was helpful to
1 thankful Users |
Follow us on