6/24/2009 10:43 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hi, It is possible to connect PC and CPU, without using a MMC. (you can not download anything to CPU). In PG/PC interface, you have selected CP5512(auto)? When you use accessible nodes, can you see address of CPU? Perhaps this link might help: Reset in the as-delivered status Best regards, Wizard |
Last edited by: Wizard at: 6/24/2009 10:52 AMLink added |
|
6/24/2009 4:12 PM | |
Posts: 9 Rating:
|
HY No DID not slecet CP5512(auto)? it does nos exist. onli PC5512(MPI)and PC5512(PROFIBUS). |
7/4/2009 6:38 PM | |
Posts: 9 Rating:
|
HY Jes I can use Diagnostics button When I press Reade it show mi just one aderse addresses. In Attachment I made picutre of diagnostic. |
Follow us on