(0)| 8/3/2024 7:55 PM | |
|
Posts: 1 Rating:
|
Hello Siemens Friends, I am using CPU 1517F-3 PN/DP as an adapter to talk to Compact logics "Scanner" using LCCF_EnetAdapter FB Question1: Can i configure two instances of LCCF_EnetAdapter FB using X1 P1 for one instance of the LCCF_EnetAdapter and X1 P2 for the second instance of the LCCF_EnetAdapter? Question2: If the answer for the above question is yes, would the interface:= parameter definition in the SCL networks below, be correct? For your convenience I marked the interface:=parameter lines with
Network2: 2nd instance of LCCF_EnetAdapter
Q3: If the answer for Q1 is no, what would be the alternative solution for having two instances of the LCC_EnetAdapter FB? If possible, please include the IP configuration/s and the SCL interface:= parameter line for each of the two instances Your input would be greatly appreciated ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/05/2024 06:45:34New subject after splitting Last edited by: Afi's Account at: 08/06/2024 13:47:22 |
|
This contribution was helpful to
|
|
Follow us on