10/22/2024 7:00 AM | |
Joined: 5/10/2023 Last visit: 7/11/2025 Posts: 3 Rating:
|
Hello Nicolas P., Currently, I find myself in the same situation as you. I have certain library blocks developed to obtain memory addresses from the HW constant (I usually use IFM IO-Link masters). For a particular project, I had to use SM 1278, 4 X IO-LINK MASTER (6ES7 278-4BD32-0XB0) on an S7-1200. Now I have to rethink the functionality of these blocks because I can’t find an HW constant associated with the IO-Link master’s port, only with the entire master. Is there any method to obtain the HW address of a specific port? Thanks a lot, Jan. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/22/2024 08:12:25New subject after splitting |
|
Follow us on