11/8/2024 6:06 AM | |
Joined: 3/30/2020 Last visit: 9/17/2025 Posts: 5459 Rating:
|
The instruction set for the S7-300 / S7-400 has an instruction for that type of function. In Step7 Classic indicates that as a unique instruction. The inline output -(#)- . As demonstrated by your screen capture.. Step7 in TIA Portal uses that instruction but just do not tell the user that the inline output is used. Refer to SIMATIC STEP 7 V5.5 Ladder Logic (LAD) for S7-300 and S7-400 Programming. An extract is attached for your review. All LAD code translates to STL code before being compiled to machine code (S7-300 / S7-400). Therefor the equivalence is..
Attachmentmidline output.pdf (235 Downloads) |
Last edited by: qwazee at: 11/08/2024 06:11:15Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
11/8/2024 6:11 AM | |
Joined: 1/17/2023 Last visit: 7/19/2025 Posts: 5 Rating:
|
Hello. Thank You for Your help! |
Follow us on