11/12/2024 8:38 AM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35946 Rating:
|
SSP SINAMICS G120 V4.7 SP14SSP for updating existing STARTER or also SCOUT installations Latest SINAMICS STARTERYou can download the latest version of STARTER via: 26233208 OSS note on SSP SINAMICS G120 V4.7 SP14Third-party software - license conditions and copyright notesYou can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file: Read_OSS.zip (22,3 KB) Special note for resellers Availability of OSS source code |
This contribution was helpful to
1 thankful Users |
Follow us on