11/13/2024 6:26 AM | |
Joined: 3/30/2020 Last visit: 9/9/2025 Posts: 5434 Rating:
|
Several methods are possible. Each method has its place with pros and cons. Difficult to say which method suits you best since you have not provided much detail. Assume the source project is of the same TIA version as the destination project. Simplest method is to open one session of TIA for the source. Open a second TIA session for the destination. Copy-paste or drag-drop the effected blocks from source session to the destination session. Variation on the theme is to open the source project as read-only reference. Use [View > Reference Project] to enable the functionality. Other methods: 1) Export STL / SCL / DB / UDT source to ASCII text files. Reimport the text into the destination project. 2) Use TIA Openness to export/import XML files. 3) Use the Project/Global Library functionality. This is a good idea for repeated re-use.
VIDEO: How do you open, edit and upgrade global libraries in the TIA Portal? |
Last edited by: qwazee at: 11/13/2024 06:30:07Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
Follow us on