11/25/2024 4:05 PM | |
Joined: 4/28/2015 Last visit: 5/15/2025 Posts: 7 Rating:
|
May not be correct thread but here goes... Needing to get a list of all objects with security placed on them and what level that security is. Is this possible or do I have to go to each screen and each object and check? This would be very time consuming. Using TIA Portal V15.1 and V16 and TP comfort HMI panels ------------------------------------------------------------------------------------------ |
Last edited by: GeoBoni at: 11/25/2024 16:07:32Last edited by: Moderator_Lan at: 11/25/2024 21:56:44New subject after splitting |
|
11/26/2024 9:58 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi GeoBoni, I'm afraid there is no direct integrated option that can perform this functionality. It would just be left to go about performing it individually to test it. Even so, there might be some option to export the project data and then analyze it externally to know the security options of these objects by column. But I do not know how to do it or if it can be done. |
If this Information really helps, you could use the Rate function |
|
Follow us on