11/8/2024 11:41 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello dan.v. You can use the event of a systemalarm to do something: (does not work for Basic Panels!) And you have to do soemthing to receive Login Information as messages: https://support.industry.siemens.com/cs/de/en/view/109758223 Bye Murof |
Last edited by: Murof at: 11/08/2024 11:41:32If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
11/22/2024 10:30 AM | |
Joined: 11/22/2024 Last visit: 12/10/2024 Posts: 2 Rating:
|
Hi. I am newbie with TIA and I am facing the same issue. Unfortunately, in Events, I only have the message "The selected object has no events" :( Does it mean I am on a "Basic Panel" ? I work with a KTP700 Basic... If so, any way to inform the user that password is wrong ? I have the same kind of issue when I try to change the password. If the new password does not respect the password complexity, the user is not informed and the password is not changed... Thanks |
11/26/2024 3:46 PM | |
Joined: 11/22/2024 Last visit: 12/10/2024 Posts: 2 Rating:
|
Ok. Thank you. Chris |
Follow us on