12/6/2023 6:26 PM | |
Joined: 12/18/2014 Last visit: 9/11/2025 Posts: 35953 Rating:
|
Download and installation instructions for LOGO! Soft Comfort Upgrade V8.4Installation instructions for the LOGO! Soft Comfort V8.4 Upgrade The LOGO! Soft Comfort Upgrade includes:
Improvements/changes for LOGO! Soft Comfort V8.4:LOGO! Soft Comfort V8.4:Support for LOGO! basic devices V8.4 and predecessor versions
LOGO! Integrity Tool:For checking the integrity of the installed LOGO! Soft Comfort V8.4 and LOGO! Web Editor V1.2 LOGO! 8.4 basic devices:
|
This contribution was helpful to
4 thankful Users |
11/26/2024 5:04 PM | |
Joined: 11/18/2024 Last visit: 11/26/2024 Posts: 1 Rating:
|
hi, how do i download the upgraded version of logo! soft comfort? i don't find a download link anywhere |
11/26/2024 5:27 PM | |
Joined: 12/18/2014 Last visit: 9/11/2025 Posts: 35953 Rating:
|
The link above is no longer active because there's a newer software and hardware update. Here's the Link: Firmware update for LOGO! 8.4 basic devices and service pack 1 for LOGO! Soft Comfort V8.4This free update contains the following individual packages: Upgrade LOGO! Soft Comfort V8.4.1 Upgrade LOGO! Web Editor V1.2.1 Firmware update for LOGO! 8.4 basic devices V1.84.03 At the end of this article, you can perform a download for the entire data package or for LWE and Firmware update individually. Changes/improvements in LOGO! SoftComfort V8.4 SP1:
Changes/improvements in LOGO! Web Editor V1.2.1:
Changes/improvements for LOGO! firmware V1.84.03: The firmware update can only be performed on LOGO! 8.4 basic devices with firmware version V1.84.01 and V1.84.02
Status: 10/25/2024 |
This contribution was helpful to
2 thankful Users |
Follow us on