4/29/2022 9:40 PM | |
Joined: 12/10/2021 Last visit: 10/4/2023 Posts: 1 Rating:
|
Dear All, I am new to S7-1200 programming and I am working on a project which involves communication between an S7-1200 and a KTP Basic Panel (there are no other ethernet/profinet devices - the two connect directly with a cat 6 cable I have confirmed to be good). My problem is that the two refuse to connect with each other despite having set up IPs and the connection appearing in the "connections" selection of TIA portal. The HMI does not display the values I want (it just shows ######## on the number field) and whenever I try to write a variable on the PLC the HMI gives me a "Could not access XXXX on the PLC" error. Both devices accept my uploads. What I am I doing wrong? One peculiarity I've noticed is that whenever I upload the PLC program to the PLC, even though the new device name is slave_1 the TIA Portal upload manager finds it as slave_3 (a previous name). Does this have anything to do with it? I am using TIA Portal v17 basic without updates and have also downloaded PLCSIM and the panel images. Attached you will find the project files on my google drive. The problem appears between the "Slave_1" PLC device and the "Slave HMI" Panel. [snip] Thanks a lot, Thalis Paktitis AttachmentNew Master-20220502T085854Z-001.zip (535 Downloads) |
Last edited by: Jen_Moderator at: 05/02/2022 11:01:08Link removed and added file as an attachment. |
|
4/29/2022 10:59 PM | |
Joined: 8/12/2021 Last visit: 8/20/2025 Posts: 351 Rating:
|
Hi Just to be on the safe side, you should update to the latest version available.
|
If this Information really helps, you could use the Rate function |
|
2/13/2024 10:10 AM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello In newer FW Version this is always a thing you have to care about: https://support.industry.siemens.com/cs/de/en/view/109803668 and check also the Date/Time on both sides (HMI and PLC) because of the Certificate validity in case of secure communication Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
11/28/2024 1:17 PM | |
Joined: 12/14/2011 Last visit: 7/24/2025 Posts: 176 Rating:
|
After follow the Siemens indication in the link: Connecting older HMI to S7-1500/1200 with newer firmware my KTP400 BASIC (firmware 17.0) however didn't communicate with S7-1200 (firmware 4.6). I downgrade the HMI firmware from 17.0 to 16.0 and all works fine. I have TIA19 update 3. Hope to be useful. Ciao. |
Last edited by: gigi_plc at: 11/28/2024 13:18:51 |
|
Follow us on