11/29/2024 4:32 PM | |
Joined: 1/2/2018 Last visit: 1/19/2025 Posts: 2 Rating:
|
i have 5 running logo! devices already for years 4*Relay,10A input 8*AC/DC AC/DC 115-240V i bought at about the same year, some 4 years ago a 6th logo! but it was in the closet. 6ED1052-1FB08-0BA1 they are all the same type of LOGO! i was running fine on software version 8.2 with these 5 logo's. i used v8.2 but i was not able to upload/download a program for the sixth logo which i try to put in production next to the 5 running ones. After upgrading to v8.3, it was not a problem to upload/download a program. strange, but thanks to old tickets i saw that this was a solution, and indeed it is. i still have a problem doing an online test, it says: online test failed. The hardware type of LOGO! in LOGO!Soft Comfort does not match with that of the connected LOGO! device. How do i match that please ? tell it please in a very simple way, with screenshots if possible with online settings, i see , firmware version: 1.83.01 the older already long running logo! showed version 1.81.03, hardware type LOGO!8.FS4 after uploading/downloading again i could see that it changed the version to LOGO!8.3 between brackets [], then i was able to do an online test ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 12/02/2024 09:41:28New subject after splitting |
|
Follow us on