12/3/2024 8:40 AM | |
Joined: 1/13/2021 Last visit: 9/13/2025 Posts: 2 Rating:
|
Dear everyone. I am working on a WinCC Advanced program that displays 18 temperature measurement points and setpoints for each point. The X axis is 1 to 18, and the Y axis is the temperature of each measurement point. I refer to the example: https://support.industry.siemens.com/cs/document/109481693/creating-an-f(x)-trend-view-for-comfort-panels-and-wincc-runtime-advanced?dti=0&lc=en-VN My program will call VBScript (attached) to save the values to SQL database and display the trend of the measurement value and setpoint on the same graph, every 5 seconds. However, sometimes I lose data when saving to SQL, leading to an error in displaying the trend (as shown in the picture). According to my observation, this phenomenon (maybe) is cyclical. I also tried increasing the VBScript call time to 10 seconds but the error still occurs. I hope to get everyone's help. Thanks so much.
AttachmentTrend.txt (148 Downloads) |
Last edited by: NEris26 at: 12/03/2024 08:42:20 |
|
Follow us on