(0)| 2/6/2025 8:43 AM | |
|
Joined: 2/17/2020 Last visit: 1/16/2026 Posts: 1251 Rating:
|
Hi, As far as the S7-1500R/H is concerned, please note that by default (simulating or with real hardware), the project data is downloaded to the primary CPU. You need right-click to select the S7-1500R/H system in the project tree, and when the "Extended download" dialog appears, the "Select target device" table will show both CPUs in the S7-1500R/H system and their roles. However, the primary CPU should already be selected. Points to consider when simulating an S7-1500R/H system can be found in this section of the PLCSIM Advanced manual: Simulating a redundant S7-1500R/H system Hope that helps! |
|
A rating will be well appreciated. |
|
Follow us on