2/20/2025 9:56 PM | |
Joined: 4/11/2022 Last visit: 8/26/2025 Posts: 90 Rating:
|
Hi mate! It is not possible to increase the final value, but you can put in line more than 1 counter. Find attached my suggestion. Use the simulation mode to make a test. Just for a test, in a first counter the limit was 5, and the second was 10... The problem is to sum all the values, it is not possible, because Math functions will not reach this big number... suggestion, change to S7-1200. Attachmentexample counter in line.zip (131 Downloads) |
Rgds, |
|
2/21/2025 4:10 AM | |
Joined: 12/18/2014 Last visit: 9/2/2025 Posts: 35912 Rating:
|
Take a look at the attached program. You can count from 1 to 999.999.999.999. AttachmentCounting_more_than_999.999_0BA8.Standard.zip (137 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on