3/8/2025 8:06 AM | |
Joined: 1/28/2009 Last visit: 9/15/2025 Posts: 6875 Rating:
|
Dear forum user, I will attach the list of all STEP 7 error code in the attachment , your error message is not listed there. There are 2 options IMHO: 1- When you encounter the message ,check the STEP 7 remedies that are available under Details or help on this error. 2- Find the original project , in folder ApiLog open the Step7Bas.ver with notepad. That is a document of the developer PC while programming the project. Try to create a machine (virtual/actual) like the original developer and open it again. Kind regards, hdhosseini Attachmentstep7_errorcode_e.pdf (226 Downloads) |
Follow us on