3/11/2025 8:35 AM | |
Joined: 3/12/2024 Last visit: 8/15/2025 Posts: 183 Rating:
|
Please have a look into our How to setup IOT2050 with IndOS to get detailed information. Instead of using SSH via PuTTY. Can you please connect an UART cable for serial connection or a keyboard and DP monitor to access the device? Try to connect from there. -> Example Image should be accessible via SSH by default / IndOS only after first commissioning. username / password should always be root by default. Please also check your keyboard settings. As the username / password is not working all the time I assume you are booting from the IndOS maybe? Please also try to download a fresh V1.3.1 Image from our Download Page and write in on the SD card. BR |
Follow us on