3/17/2025 9:07 AM | |
Joined: 2/22/2024 Last visit: 9/11/2025 Posts: 3 Rating:
|
Hi everyone, I'm working with TIA Portal V20 and S7-PLCSIM V20. My setup includes an ET 200SP, CPU 1512SP F-1 PN, and my HMI is a TP1200 Comfort Panel, connected to port X2. The issue I’m facing:
What I have checked so far: Note: Two weeks ago, when the setup was here, i simulated the HMI on the PLC, and everything worked fine. Has anyone encountered this issue before? Any suggestions on what might be causing this? Thanks in advance! AttachmentScreenshots.zip (226 Downloads) |
Last edited by: Jelle_Lippens at: 03/17/2025 09:07:57 |
|
3/17/2025 9:09 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
check your PG/PC Setting in Windows Control Panel |
This contribution was helpful to
1 thankful Users |
3/17/2025 9:26 AM | |
Joined: 2/22/2024 Last visit: 9/11/2025 Posts: 3 Rating:
|
Already checked that, should be fine as is. |
Follow us on