4/4/2025 9:14 PM | |
Joined: 9/21/2024 Last visit: 5/14/2025 Posts: 8 Rating:
|
Hello dear friends, I have a KTP1200 panel that I control remotely via a SIM card modem and via the Smart Client application and static IP, but my problem is that after a few hours to a maximum of a day, my access to the panel is cut off, but when I disconnect and reconnect the power to the panel (in this case, none of the IP and default gateway settings have changed, etc.) the panel is still available for a while in the same state as I said. In the modem settings, DHCP is turned off, please help me. Best Regards Navid ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 04/07/2025 07:10:27New subject after splitting |
|
4/11/2025 11:42 AM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello navid_neshat56 the best you can do is to use the latest OS Version for you Panel (should be V17.0.0.8). Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on