4/15/2025 1:53 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
That works. I can also connect my old 0BA5 to LSC V8.4.1 (the current LSC version). |
4/15/2025 2:25 PM | |
Joined: 2/20/2025 Last visit: 5/27/2025 Posts: 5 Rating:
|
HelloElla68, Yes,I have the cable for logos and I've always managed to connect on others. Pascal |
4/16/2025 10:11 AM | |
Joined: 6/11/2019 Last visit: 8/31/2025 Posts: 2623 Rating:
|
Hello pascal88, To get up to date, download the latest upgrade here. You'll need to activate your account first (if you haven't already). Then install your old full license and then the upgrade. I'm not familiar with Windows 10 anymore, but isn't it possible to force 32-bit mode for certain programs? If all else fails, you could set up a VM running an older 32-bit version of Windows that's tailored specifically for Siemens software. You'd also have the advantage of having everything running in a secure location, allowing you to quickly create a backup at any time. Regards, Ella_68 (translated by Google) |
This contribution was helpful to
1 thankful Users |
4/16/2025 10:38 AM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
If you do not have a full version of LSC installed on your Windows 10 PC, you can install the downloaded upgrade to LSC V8.4.1 with the V3.1 CD using these instructions: How do you install a downloaded upgrade for LOGO!Soft Comfort with or without installed LOGO! software? |
This contribution was helpful to
1 thankful Users |
Follow us on