5/6/2025 8:41 AM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16461 Rating:
|
Hello Tech Ahmed you could try to use the systemfunction "StartNextLog" in the Scheduled taks with a daily trigger you would have to use a segment that is big anough for the whole day. But keep in mind that the size of a historical data log is the sum of all entries of all segments. And the limits are defined inthe Help system. https://support.industry.siemens.com/cs/ww/en/view/109815056/149280616843 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
5/14/2025 4:05 AM | |
Joined: 1/16/2012 Last visit: 6/30/2025 Posts: 127 Rating:
|
Hi Murof, I will check and try. Thanks. Best regards, Tech Ahmed |
Follow us on