4/25/2025 11:12 AM | |
Joined: 5/29/2024 Last visit: 9/12/2025 Posts: 123 Rating:
|
Hi! The following alternatives come to mind: -The manual is for WinCC V8, but it also works for WinCC Professional. You can create a script in a button to open a window. -> WinCC V8.0 Information System > OpenScreeninPopup method - You can review the following sections that inform you how to create and manage pop-ups. -> SIMATIC STEP 7 Basic/Professional V18 and SIMATIC WinCC V18 > Working with pop-up screens Hope it helps! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
Follow us on