6/10/2025 5:53 AM | |
Joined: 6/10/2025 Last visit: 7/18/2025 Posts: 4 Rating:
|
I’ve been working on establishing an MQTT connection from my Siemens LOGO! PLC (using LOGO! Soft Comfort v8.4) to a registered Zoho IoT device that includes proper credentials (username, password, and TLS settings). However, I consistently encounter a “Failed to parse” error when attempting to connect to Zoho’s MQTT broker. Interestingly, when I configure the same setup to connect to a local Mosquitto MQTT broker, the connection is successful. This confirms that the basic MQTT configuration on the PLC side is functional. Given this, I'm unsure what's blocking the connection specifically to Zoho’s broker. Could it be due to:
Any guidance or suggestions to help troubleshoot or work around this issue would be appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 06/10/2025 09:32:43New subject after splitting |
|
6/10/2025 9:33 AM | |
Joined: 7/30/2024 Last visit: 9/15/2025 Posts: 949 Rating:
|
Topic closed because the question has been posted twice. The active topic can be found here: Issue Connecting Siemens LOGO! PLC to Zoho IoT via MQTT (Soft Comfort v8.4)
Kind regards, Moderator_Lan |
Follow us on