6/16/2025 11:46 AM | |
Joined: 12/18/2014 Last visit: 9/19/2025 Posts: 36021 Rating:
|
I tested with LSC V8.4.0 and LSC V8.4.1 and a LOGO! 8.0 (6ED1 052-1MD00-0BA8). I can without problems download a program from the LOGO! to the PC and also upload a program from the PC to the LOGO!. My suggestion: Create a Support Request. |
This contribution was helpful to
1 thankful Users |
6/16/2025 4:39 PM | |
Joined: 3/1/2025 Last visit: 8/24/2025 Posts: 4 Rating:
|
From where did you get the software? I think I might have to reinstall Logo Soft. |
6/16/2025 5:00 PM | |
Joined: 12/18/2014 Last visit: 9/19/2025 Posts: 36021 Rating:
|
If you have no original installation CD or DVD then must you buy a new CD or DVD. |
Follow us on