7/15/2025 6:50 AM | |
Joined: 10/31/2022 Last visit: 8/7/2025 Posts: 1 Rating:
|
Hi, I have a WinCC Advanced-based runtime system that logs data from three PLCs via MPI to the runtime PC using a CP5711 communication processor. The data is logged to a database, which is connected to an MS SQL Server. A total of six data logs are configured, each using the database as the storage location with a circular logging method. The acquisition mode is set to cyclic. Logging cycles vary—some logs are configured for a 2-second interval, while others operate at a 1-second interval. Problem: Please support us to resolve the issue. please refer the attached PDF for more info AttachmentData logging issue.pdf (67 Downloads) |
Follow us on