8/20/2025 1:25 PM | |
Joined: 8/3/2009 Last visit: 9/4/2025 Posts: 16338 Rating:
|
Hello Sergio Massao often the errors with the missing startscreen indicates configuration issues. you can check also this FAQ (its expecially for WinCC Prof): https://support.industry.siemens.com/cs/ww/en/view/108464289 Also do you have created the lmhosts files on the system like mentioned in the FAQs? (you should do this also if the name reesolution works somehow with windows functionalities) You use a very old TIA Portal Version... which OS do you use exactly (with build number)? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on