8/21/2025 6:01 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello AutoGen_6674958 you have to seperate between an engineering license (here WinCC Advanced is available also up to V20) and the Runtime license (the latest Version and also license for WinCC Advanced RT is only available up to !!V17!!). So the best would be you by an upgrade of the runtime License up to V17 and in the TIA V20 project, you set the Device Version of your WinCC Advanced Runtime to V17 (newest you can set) A good overview to all licenses is in the delivery release in the orderdata excellist: https://support.industry.siemens.com/cs/de/en/view/109963793 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on