12/23/2020 10:51 AM | |
Joined: 4/7/2017 Last visit: 8/2/2024 Posts: 1 Rating:
|
Hi! When i switch TCP/IP Communication from <Local> to local connection(my ethernet adapter of course), i see an error "Virtual switch setting could not be applied. Please close all network interface property windows". My Realtek Adapter and Siemens PLCSIM Virtual Ethernet Adapter are in the same network. Checkbox "Siemens PLCSIM Virtual Switch" is checked on both adapters. Screenshots attached [snip] AttachmentFiles.zip (791 Downloads) |
Last edited by: Jen_Moderator at: 12/27/2022 12:43:19Link removed and all files added as attachment. |
|
8/4/2021 5:45 PM | |
Posts: 3 Rating:
|
Hi, I also have the same problem. Have you solved it? |
This contribution was helpful to
1 thankful Users |
12/27/2022 10:36 AM | |
Joined: 11/12/2014 Last visit: 6/27/2025 Posts: 1 Rating:
|
Hello, I also have the same problem too... you have a solution? |
8/21/2025 8:59 AM | |
Joined: 2/11/2023 Last visit: 8/21/2025 Posts: 26 Rating:
|
Can you provide a picture of your setup? |
Follow us on