9/11/2025 7:47 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16438 Rating:
|
Hello Falcc I would try to do a reset of the temp data: https://support.industry.siemens.com/cs/de/en/view/109778709 Then do a full compile and check if there are any errors or warnings in the info window Which Device version do you have selected for the panel,, do you use the latest V12 which is available for this kind of Panel (Basic Panel 1st Generation). Can you load a new test project to the panel (perhaps only with a Exit Runtime Button) or is it the same behaviour? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on