9/16/2025 8:51 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16437 Rating:
|
Hello So what have you done so far? Did you get managed to print the PDF already? Use a Report and a Button in your HMI to ceate the pdf file, this should work straight forward. Unfortunately there is not ready event or similar with which you can synchronize your copy job to the netshare. you can also try to pint directly on the networkshare but then you have to use SMB1.0 and the conventional integration of the networkshare. https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on