7/21/2009 7:18 AM | |
Posts: 288 Rating:
|
Hi all, Can some one please tell me if it is possible to use SIMATIC IT Historian along with WinCC only,(not PCS7).This isthe requirementof one of our clients |
7/21/2009 9:07 AM | |
Joined: 9/27/2006 Last visit: 9/11/2025 Posts: 12407 Rating:
|
Hello Yoga; The following FAQ discusses the connection of IT Historian with WinCC and WinCC Flexible, and also with standalone .csv files. So you should have no problem with your application. http://support.automation.siemens.com/WW/view/en/28398089 You will have to decide whether the suggested add-on for WinCC (Historian Connect Alarm) is what your project requires, but it garantees connections to a number of WinCC applications and a specific throughput level with IT Historian. Unfortunately, the link proposed at the bottom of the FAQ page doesn't seem towork. Here is another one that will show you more information on available add-ons for WnCC: https://www.automation.siemens.com/hmi/html_76/products/software/wincc_addons/index.htm Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/21/2009 9:26 AMLast edited by: dchartier at: 7/21/2009 9:23 AM |
|
Follow us on