7/23/2009 5:18 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hi Pl see the attached extract from ST50 catalog which gives the wiring and technical details of both module types.. The 4UA.. AO module is capable of +/- 10V and 0-20mA Output However 4UB.. AO Module can only give +/-10V Output So if you are using only voltage outputs you can use 4UB.. also but not if you have mA Analog outputs used. I hope this helps Best Regards Navnag Attachment6ES5_470.PDF (504 Downloads) |
There is no such thing as the last bug in a program |
|
7/24/2009 11:12 AM | |
Posts: 77 Rating:
|
yess sir! thanks a lot, its so helpful. |
Follow us on