7/14/2009 2:16 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
The selection from Step7-hardware-catalogue (GSD-file) allows only 10 PZD. 16 PZDs are only possible when selecting the drive(s) with DriveES - functionality. This is provided by installation of option-package DriveES Basic. http://support.automation.siemens.com/WW/view/en/34319226 |
This contribution was helpful to
1 thankful Users |
7/20/2009 6:40 AM | |
Posts: 22 Rating:
|
Hi.. You means to say that if Iuse drive ES than I can transmit and recive 16 words with PLC? Regrads, Dipak |
7/21/2009 4:17 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
Yes !! |
7/22/2009 10:25 AM | |
Posts: 37 Rating:
|
I am also trying with the same solution posted , but i am unable to configure drive with 16 PZD in hardware configuration with CPU 414-3DP. What exactly i have to do with DRIVE ES AttachmentHW configuration_pdf.pdf (609 Downloads) |
7/27/2009 12:08 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
Please see attachment and compare the 2 screen-shots: Switch (pull-down menue, little arow on right side/end of PPO5....... ) from PPO5 to none and create input-slot with 16 pzd and output-slot with 16 pzd. AttachmentDES.zip (586 Downloads) |
7/29/2009 6:35 AM | |
Posts: 22 Rating:
|
Thanks for the solution.... |
Follow us on