7/30/2009 9:29 PM | |
Posts: 2930 Rating:
|
Hi, I'm not an expert in Modbus, but the EM241 only works as a modem. So I expect that it can communicate but only vie telephone line. If you want to connect directly then: + have a look to Tip41 (secodn CD of Micro/WIN or Siemens Internet) + goto: http://support.automation.siemens.com/WW/view/de/27832511 + Modbus Slave simulation for PC, go to http://www.s7-200.net I hope this helps |
This contribution was helpful to
1 thankful Users |
8/1/2009 11:06 AM | |
Posts: 2 Rating:
|
Tomy Master and Helmut_13 thanks for u help. As I understood for Modbus need use only freeport on CPU, and no solution for use ~communication module for cpu ? |
Follow us on