8/4/2009 11:21 AM | |
Posts: 12 Rating:
|
Hi, Thanks for the reply, i have attached an extract of the program for you to take a look at. If i'm getting this right, i need to call the interrupt using the ATCH command and specify the enable bit which should be the input which sets the alarm (I0.4 in the program). I'm assuming then i need to move all the bits associated with this code to different memory locations to allow it to operate in the INT_0 pou? Thanks again Dan AttachmentAlarms.zip (287 Downloads) |
Follow us on