8/4/2009 1:50 PM | |
Posts: 691 Rating:
|
Hope you are using Step 7 Professional Version The Download Button is enabled in the Basic Version Please Refer the attached Picture |
8/4/2009 4:02 PM | |
Joined: 11/15/2006 Last visit: 3/26/2025 Posts: 1319 Rating:
|
Hi Ninja Robot, this is due to project settings set to PCS7. See http://support.automation.siemens.com/WW/view/en/19267653, point no. 2. This often occurs after installation of an optional software package which is in general used in PCS7 only as PDM. |
Have Fun! |
|
This contribution was helpful to
8 thankful Users |
Follow us on