(0)| 7/31/2009 9:19 AM | |
|
Posts: 30 Rating:
|
I have to change a damaged MIDIMASTER vector drive with a new MICROMASTER 440 because midimaster is no longer available.The problem is with the parameters beause are not the same.I changed the basic parameters like motordata but i still have problems.i would apreciate any help Below i give the .dnl file of the midimaster drive AttachmentN -(midi).zip (265 Downloads) |
| 7/31/2009 2:25 PM | |
|
Posts: 739 Rating:
|
please open an srevice request at the Hotline, they can help. sdsupport.aud@siemens.com |
| 9/4/2009 9:51 PM | |
|
Posts: 4 Rating:
|
I hope that this issue is solved already by now - however if you are still having issues there is a spreadsheet that allows you to enter the MM3 parameters into it and get MM440 parameters out. It does not manage 100% of the parameters but for the majority of users it will suffice. For any that it doesn't work for, the hotline can of course help.
AttachmentAutomated MM3V to MM440 Parameter Conversion 100103.zip (316 Downloads) |
Follow us on