(0)| 11/8/2009 3:43 PM | |
|
Posts: 39 Rating:
|
Hello! So can I use the following architecture annexed? Can I use Profibus CP with the IM153-2? The CP in the ET200M must be master, to connect with the gateway. Thanks, Rodrigo AttachmentArchitecture.pdf (317 Downloads) |
| 11/9/2009 1:45 PM | |
|
Posts: 5822 Rating:
|
Dear Rodrigo, I am sorry for the simple answer... but I say: No. Best regards J_Bell |
| 11/9/2009 3:56 PM | |
|
Posts: 39 Rating:
|
Dear J_Bell, OMG man I am really lost.... So instead of using CP342-5, can I use CP341 (modbus)? Changing the gateway too for sure. Thanks, Rodrigo |
| 11/10/2009 3:29 PM | |
|
Posts: 5822 Rating:
|
Dear Rodrigo, I think this should work, but here I would use the CPU DP interface as DP Master instead of the CP, the CP may be used for the HMI connection. But, in this special case I have to say that I am not sure how the functions needed for the MODBUS communication work in the redundancy case... this would be something to be verified. Best regards J_Bell |
This contribution was helpful to
|
|
Follow us on