(0)| 11/21/2009 4:59 AM | |
|
Joined: 8/23/2009 Last visit: 4/25/2025 Posts: 5 Rating:
|
Hi Guys, I am currenly using PCS7 v7.0 SP2 with F-Systems v6.0. Whenever I do a changes only download to two of my CPU's I get an error saying "System Error (1739:60458)" - Online CPU handle invalid. This error prevents the download from happening and the CPU starts flashing all the LEDs. The CPU then goes into STOP mode or sometimes the F-Systems falls over and I have red exclamation marks on the function blocks. Im not sure what has caused this to happen or what I canI doto resolve this? Please see attached files for errors. I also experienced a strange error recently but this one has only come up once "Initialization Error" Any feedback will be helpful. Thanks in advance AttachmentErrors.zip (274 Downloads) |
Follow us on