(0)| 1/20/2010 11:33 PM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello deepak.samal05, I
I understand you are planning to build a connection between 2 or more S7-400 PLCs, right? What's theamount of data that you want to exchange? What CPUs and communication processors do you have? Maybe you should try this sample program, Edit, I'm quite sorry. I thought you needed help regarding communication between PLCs. Client/Server terminology is used sometimes to describe PLC communicating partners. I'll ask moderators to move this thread to PCS7 conference in order to get more answers and more support. In addition to what Wavehas already told you,I hope you will find the following FAQ helpful, How do you create a SIMATIC PCS 7 V6.0 SP3 project with S7-400 station, pair of redundant servers and client? Best regards. H-H |
Last edited by: H-H at: 1/21/2010 9:37 AMLast edited by: H-H at: 1/21/2010 12:18 AMSample program has been added |
|
| 2/5/2010 4:41 PM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi deepak.samal05 , sorry for late, this link should help you to start How do you create a SIMATIC PCS 7 V6.0 SP3 project with S7-400 station, pair of redundant servers and client? regards |
Follow us on