(0)| 2/14/2010 11:23 AM | |
|
Posts: 49 Rating:
|
Hi why and where we use the direct torque control(DTC), ? do we need feed back? regards nadeem |
| 2/16/2010 10:48 AM | |
|
Posts: 739 Rating:
|
Hi nadeem, In addition to a wide range of applications where drives are used to control the speed (variable-speed drives), there are also numerous cases where it is necessary to control the drive torque. Typical applications for closed-loop torque controls are as follows Axial winder: Axial winders are used to wind and unwind material webs, cables, wires etc. Constant speed is not decisive – but instead constant tension over the complete winding range. The tension is controlled using a dancer roll, with tension measuring transducer or indirectly using the motor torque. See ….. http://support.automation.siemens.com/WW/view/en/23939668 http://support.automation.siemens.com/WW/view/en/7714804 (http://en.wikipedia.org/wiki/Direct_torque_control) ….. and attachement. Attachmentprinciples of inverter.pdf (616 Downloads) |
This contribution was helpful to
|
|
| 2/17/2010 8:57 AM | |
|
Posts: 49 Rating:
|
Hi-jens thanks for sending the good information regards Nadeem |
Follow us on