2/22/2010 8:49 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Ok, When starting with 7.1 with CFC, I was toying with some blocks->imported them in CFC but did not use them. I want to use the clean up function, because I want all the blocks that are not used in CFC charts, be gone. I'm a perfectionist, so only want the blocks I used;) But, like always... is this function safe to use? Not like the "Optimize Run time sequence" function that can screw up your program? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on