(0)| 2/15/2010 3:47 AM | |
|
Posts: 3 Rating:
|
Dear Experts, I am working on a project in which I need to communicate to a remote static IP address with the help of SINAUT MD720-3. I have seen a similar application here:
To give a brief description, I have a CPU 315- 2PN/DP connected to a CP 340 via back plane bus on a rack. CP 340 is connected to MD720-3 with a serial cable. The MD720-3 has a GPRS enabled SIM card. I need to send data from a DB (DB1 for example) to a remote computer with a static IP. This remote computer will have an application running which will capture the data coming to the computer through TCP IP socket. The problem I am facing is that I am unable to make the CP 340 send anything through the help of WDC_SEND of the GPRS library which is given in the above mentioned application.I tried to go through the code of the program given to modify it according to my requirements, but it was in German and I could not understand most of it. Can you please let me know if there is a program which enables me to do the above communication easily. If you can send me the GPRS library in English and the instructions to use it in a program it will be extremely helpful. Anything which will make my project successful will be highly appreciated. Also 1 question is that, in the GPRS library manual, its mentioned that WDC_SEND and WDC_RECV are KNOW-HOW protected. But in the above given example, I am able to access both the blocks. Can you please let me know if its theoriginal WDC_SEND and WDC_RECV blocks that is being used in the program or has it been modified? It will be helpful if you can provide a simple application which initializes the SINAUT MD720-3 modem and should be able to send simple GPRS commands. Thanks in advance, Hoping to get a positive reply |
Last edited by: vinayl at: 2/15/2010 7:29 AMLast edited by: vinayl at: 2/15/2010 7:28 AMAdded 1 more question |
|
Follow us on