(1)| 6/11/2010 2:54 PM | |
|
Posts: 739 Rating:
|
please find the answer in FAQ: http://support.automation.siemens.com/WW/view/en/22978972 |
| 6/11/2010 2:57 PM | |
|
Posts: 739 Rating:
|
dearating tables please find in the mauals; for power losses please see FAQ: http://support.automation.siemens.com/WW/view/en/22978972 |
| 6/11/2010 3:20 PM | |
|
Posts: 112 Rating:
|
dear jenss, thanks for reply,but you given bothFAQ link not open. Kindly give us reply. thanks in advance. |
| 6/12/2010 12:11 AM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, here is the text and the attachment from JensS' link Cheers, Graeme Like all electrical equipment, inverter drives produce waste heat. This heat must be removed to prevent the drive overheating. As most commercial electronics is limited to 70°C (the internal junction temperature must be limited to 125°C or 150°C, but is usually maintained below this), the maximum temperature of the cooling air surrounding, or supplied to the drive is therefore limited to 50°C. For some types and applications, this is reduced further to 40°C (see operating instructions and specification for details). It is normal to install the drives, together with other equipment, in a cabinet or similar installation. The temperature of the air inside the cabinet must therefore be calculated. In some cases, cooling air may be supplied by an external fan or ducting. In these cases, the calculation will need to account for the amount of air, as well as its temperature. As part of the design of the installation, the following steps should allow the calculation of the temperature rise, and a suitable cooling system selected. 1. Determine the total power dissipated in the cabinet under worst case conditions (= ambient temperature in the cabinet). 2. Determine the maximum temperature of the air outside the cubicle, or the temperature of the air fed to the cubicle if ducted air is used. 3. Calculate the temperature rise. If this is too high, consider a different cooling solution (see PDF_additional_text). Details to calculate the temperature and power losses are in the attached file. AttachmentPDF_power_loss_and_temperature_rise_en.pdf (344 Downloads) |
This contribution was helpful to
|
|
Follow us on