6/30/2010 8:40 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi algudkar, Here is the link you will find all the GSD File including the EM277 way you want the CP5613 GSD File? you have S7300 PLC in your configuration to communicate with WinCC V6.0, |
Ammy |
|
6/30/2010 9:07 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Algudkar, Here is the Link for the What are the options for accessing an S7-200 with WinCC? & Here is the Link for the How do you configure an S7-200 connection via PROFIBUS DP? For Second option I have never used, In that COM Profibus is the Software which is Used for the S5 Network Configuration, or If you want to SCADA Then you can used the WinCC Flexible Runtime Station also, |
Ammy |
|
Follow us on